BQT6904800 -03

Cubicle Design

The MCSeT range is available in the following cubicle layouts:

  • Feeder with Contactor Cubicle (FC)

  • Incomer or Feeder (I/F)

  • Bus Section Coupler (BSC)

  • Bus Section Riser (BSR)

  • Busbar Metering and Earthing (BME)

Figure 1
Cubicle Design

1

LV compartment

12

Cable compartment

2

P5 relay

13

VT

3

HMI screen

14

Fuse

4

Voltage Detecting and Indicating System (VDIS) and PowerLogic Partial Discharge100 (PD100)

15

Surge arrester

5

EvoPacT HVX VCB

16

Shutter

6

Handle

17

Cables

7

Switch OFF/ON push buttons of EvoPacT HVX VCB

18

Position inspection window for cables from rear window, VT and E/S position indication.

8

Access to spring charge

19

E/S

9

Access to rack-in/rack-out

20

CT

10

Operator interface of the E/S

21

Spout

11

Label of E/S manual operating instruction

22

Busbar

NOTE: The images shown here are for illustration purpose only.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?