BQT6904800 -03

Heater

WARNING
HAZARD OF equipment corrosion
  • Do not alter the location of the heater.
  • Do not tamper with the heater wires.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTICE
hazard of inappropriate storage
Indoor switchgear units must be stored in a pollution-free indoor environment.
Failure to follow these instructions can result in equipment damage.

Each MCSeT cubicle is equipped with two heaters, in the VCB compartment and in the cable compartment respectively. Refer to figure 15.

Energize the heaters to help prevent any moisture formation inside the switchgear units.

Figure 15
Location of Heater in MCSeT Switchgear

NOTE:
  • Heaters should be ON and energized for two days before commissioning or putting in service.

  • The images shown here are for illustration purpose only.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?