BQT6904800 -03

Rack-in the truck from Disconnected Position into Service Position

Follow the below steps to rack-in the truck from disconnected/test position into connected/service position:

  1. Rotate knob (1) counter-clockwise and hold it until the flap provides access to the guide. Refer to the Figure 43.

  2. Insert truck handle (3) through the opening guide in the door onto the drive shaft of the VCB truck.

  3. Turn the truck handle (3) clockwise until the truck is racked-in.

  4. Remove the truck handle (3) and place it back into the transport trolley.

  5. Check the position of the truck through the inspection glass (4).

Figure 43
Racking-in the Truck via Truck Handle

1

Rotatory Knob

3

Handle

2

Indicator

4

Inspection glass

NOTE: During the rack-in/rack-out, the door gets locked to help prevent it from opening. The door can be unlocked only if the truck is in the disconnected/test position.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?