BQT6904800 -03

Labels and Indicators

Labels and Indicators on the VCB Cubicle

Figure 8
Example of Front View Indicators of I/F Cubicle

1

Switch ON/OFF guide of EvoPacT HVX VCB

4

Rack-in/rack-out manual operating instruction

2

Single line diagram

5

Rack-in/rack-out position indicators

3

Access to spring charge

   
NOTE: The images shown here are for illustration purpose only.

Labels and Indicators on the Feeder with Contactor Cubicle

Figure 9
Labels and Indicators on the Feeder with Contactor Cubicle

1

Switch OFF guide of CVX contactor

4

Rack-in/rack-out manual operating instruction

2

Single line diagram

5

Rack-in/rack-out position indicators

3

Locking mechanism for switching device compartment door

6

Interlocking slide for manual actuation of the truck

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?