BQT6904800 -03

Padlocks

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Ensure terminals are not live before opening the shutter.
  • Padlock the shutter in close condition while performing maintenance.
  • Remove shutter padlock while racking VCB to service position.
Failure to follow these instructions will result in death or serious injury.

The holes are provided for padlock yokes of Ø 8 mm.

NOTE: All the padlocks are not included in the scope of supply.

Figure 26
Manual Switching ON of Circuit Breaker Locked by Padlock

Figure 27
Manual Switching OFF of Circuit Breaker Locked by Padlock

Figure 28
Mechanical Lock-out of Earthing Switch by Padlock

Figure 29
Padlock for the Shutter

Figure 30
Padlock for the Handle



Figure 31
Manual Switching OFF of Contactor Locked by Padlock



Figure 32
Padlock on Truck - Manual Insertion of Contactor Truck Blocked by Padlock



Figure 33
Contactor Cubicle - Mechanical Lock-out of Earthing Switch by Padlock

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?