BQT6904800 -03

Access to the Busbar Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
Before accessing the busbar compartment from rear side, ensure the following:
  • VCB in the I/F cubicle is in test/isolated position.
  • E/S of the respective cubicle is switched ON.
  • E/S/earthing device in BME cubicle is switched ON.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?