BQT6904800 -02

Transport Trolley

WARNING
hazard of inappropriate handling
Ensure EvoPacT HVX VCB handling trolley is locked with cubicle before engaging/disengaging EvoPacT HVX VCB from cubicle.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Mechanical transportation trolleys are available in two configurations for EvoPacT HVX VCB/EvoPacT MTX, based on the cubicle width:

  • 650 mm trolley

  • 800 mm trolley

  • 1000 mm trolley.

Figure 15
Mechanical Transportation Trolley for the EvoPacT HVX VCB/MTX

1

Guiding pins

8

Height adjusting wheel

2

Trolley locking arrangement

9

Body of the trolley

3

Guiding pins

10

Height adjustment arrangement at the trolley base.

4

EvoPacT HVX VCB/MTX stopper on the trolley

11

Rear wheel

5

EvoPacT HVX VCB/MTX rolling plane

12

Front wheel

6

Knob to lock the trolley

13

Operation accessories placement in the trolley

7

Locking the withdrawable part on the trolley

   

NOTE: The images shown here are for illustration purpose only.

Table 9 Trolley Variants

Rated volt-age Ur of the panel (kV)

Panel width (mm)

Trolley

Reference

View

12/17.5

650

EvoPacT HVX VCB/MTX

PG9CBTLY06S3703

800

EvoPacT HVX VCB/MTX

PG9CBTLY08S3701

1000

EvoPacT HVX VCB/MTX

PG9CBTLY10S3702

24

800

EvoPacT HVX VCB/MTX

PKR8468001

1000

EvoPacT HVX VCB/MTX

PKR84175

NOTE: The images shown here are for illustration purpose only.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?