BQT6904800 -03

BSC-BSRCubicle

Figure 4
BSC-BSR Cubicles

1

Busbars

8

Rack-in/rack-out

2

Handle

9

Position inspection windows of the withdrawable part

3

Switch ON/OFF push button of EvoPacT HVX VCB

10

EvoPacT HVX VCB compartment

4

Rating plate

11

VDIS

5

Operator interface of the E/S

12

PowerLogic PD100

6

Label of E/S manual operating instruction

13

LV compartment

7

Position inspection window for VT

   
NOTE: The images shown here are for illustration purpose only.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?