BQT6904800 -03

VDIS

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION, OR ARC FLASH
  • You must use the VDIS unit to detect and indicate the presence or absence of operating voltage.
  • You must not use the VDIS unit to distinguish between voltage not present (i.e. U < 10% of nominal voltage) and dead circuit state (i.e. U = 0 V).
Failure to follow these instructions will result in death or serious injury.

The VDIS unit is a self-powered device.

The VDIS unit is integrated into MCSeT cubicles, flush-mountable and designed according to standard IEC 62271-213. The VDIS unit is fitted with a three LED display and detects the operating voltage presence or absence on the cubicle main circuit.

NOTE: VDIS is not intended to distinguish between voltage not present (that is U < 10% of nominal voltage) and dead circuit state (that is U = 0 V). The VDIS receives the information through the capacitive sensor installed inside the insulator.

The range of VDIS consists of two versions:

  • No voltage output (VO): Voltage presence detection and interface to phase concordance units.

  • VO FlairDIN: Voltage presence detection, interface to phase concordance units and VO connection to fault passage indicators.

The VDIS unit has three main functions:

  • Visual indication of MV operating voltage presence or absence,

  • Phase concordance output,

  • VO (VDIS-VO only).

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?