BQT6904800 -03

Operation Accessories

The cubicle may be operated using these accessories.

Figure 19
Location of Operation Accessories in the Trolley

1

Accessories placed in the trolley

NOTE: For the details of operation accessories supplied together with the MCSeT cubicles, refer to Table 11.

Table 11 List of Operational Accessories

Description

Item no.

Illustration

Double-locking bit key for the cable door and LV compartment door

SEM101137-01

Manual spring charging handle

AGS H30498-01

ON/OFF operating rod

AGS H35446-01

E/S handle

CHD1000063P0005

Truck handle (rack-in/rack-out)

CHD8000092R0162

Crank for truck

AGSH31601–01

Operating lever for earthing switch

AGSC74270–01

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?