BQT6904800 -03

BME Cubicle

Figure 5
BME Cubicle

1

LV compartment

6

MV cubicle

2

Bushing

7

Handle

3

VDIS

8

Access to rack-in/rack-out

4

PowerLogic PD100

9

Operator interface of the E/S

5

Busbars

10

Label of E/S manual operating instruction

NOTE: The images shown here are for illustration purpose only.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?