BQT6904800 -03

Access to the EvoPacT HVX VCB Compartment

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Make sure that the racking device is in disconnected/test position before opening the front door.
  • Turn off all power supply or de-energize the complete cubicle because opening any door is not allowed if the busbar or cable is live.
Failure to follow these instructions will result in death or serious injury.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?