BQT6904800 -02

Access to the Cable Compartment from Rear Side AFLR

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Rear access must only be accessed with AFLR internal arc classification.
  • Ensure the VCB is in disconnected/test or racked-out position inside the cubicle.
  • Ensure the E/S is in a closed or earthed.
  • Isolate the cubicle from the power supply.
  • Obtain work permission for zero voltage from the relevant team.
Failure to follow these instructions will result in death or serious injury.

Removal of Cable Compartment Rear Cover

Follow the below steps to open the rear cable access door:

  1. Unscrew the M8 x 25 screws (3) and remove the M8 plain washers (2) by using an Allen key. Refer to Figure 54 and Figure 55.

  2. Remove the rear cover (1).

  3. The cable compartment is now accessible from the rear side (AFLR).


Figure 55
Rear Access of the Cable Compartment 12/17.5 kV


Figure 56
Rear Access of the Cable Compartment 24 kV

1

Rear cover

2

Washer M8

3

Screws M8 x 25

NOTE: After completing assembly work, follow the above steps in reverse order to remount the cable compartment rear cover.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?