BQT6904800 -03

Switching ON the E/S

Follow the below steps to switch ON the E/S:

  1. Press the slider (2) downwards until access for the E/S operation is available. Refer to the Figure 45.

  2. Insert E/S handle (1) aligned with axis point.

  3. Turn the E/S handle (1) clockwise by 180°.

  4. Check the E/S position indicator through cable compartment inspection window and make sure that the E/S is ON.

  5. Remove the E/S handle (1) and place it back into the transport trolley.

Figure 45
Switching E/S ON

1

Handle

2

Slider

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?