BQT6904800 -03

Interlocks

The MCSeT switchgear has two types of interlocks:

  • Mechanical interlocks.

  • Electromagnetic interlocks (optional).

WARNING
HAZARD OF INAPPROPRIATE OPERATION
  • Installation, repair and maintenance work on the EvoPacT HVX VCB must only be carried out by qualified and certified personnel.
  • Ensure to comply with the operation procedures and the interlock mechanism is operated effectively. Refer to Operations and Interlocks.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

The mechanical interlocks are the primary interlocks, which is supported by an additional electrical interlock function to achieve the switchgear cubicle safegaurd interlock function.

EvoPacT racking device has a robust interlocking system with:

  • Switchgear door

  • LV plug

  • VCB

  • E/S.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?