BQT6904800 -03

Opening and Closing the VCB Front Door

Opening the Front Door

  1. Hold the door handle, and pull it upwards.

  2. Swing the door to the left side. Refer to Figure 68.

Figure 68
Access to the Main VCB Compartment


Closing the Front Door

  1. Close the door completely.

  2. Turn the handle downwards for the full stroke.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?