BQT6904800 -03

Safety Provisions

Before performing work on the cubicle, it is essential that you comply with the following instructions:

DANGER
HAZARD OF electric shock, explosion, or arc flash
Before removing covers and performing assembly or maintenance work:
  • Ensure that the system is isolated from high voltage, supply voltage, and properly grounded.
  • Ensure that the VCB is in test condition, the E/S is closed, and access is locked.
  • Follow the LOTO process to perform any work on switchboard.
  • Install barriers, cables, and polycarbonates in accordance with the design specifications wherever necessary.
Failure to follow these instructions will result in death or serious injury.
WARNING
HAZARD OF MOVABLE PARTS IN MECHANICAL DRIVES
Before performing mounting and maintenance work, comply with the below safety rules:
  • Isolate from the supply voltage.
  • Release the energy-storing device of the VCB by performing the OFF-ON-OFF operation.
  • Activate the make-proof E/S to ON position, to ensure that the equipment is ready for use (if any).
  • Do not remove the mechanisms during maintenance work.
Failure to follow these instructions can result in death, serious injury, or equipment damage.
WARNING
HAZARD OF SHARP-EDGED SHEET METAL AND METAL PARTS
During installation and maintenance work, comply with the below safety rules:
  • Apply appropriate PPE and follow safe electrical work practices. See standards or local equivalent.
  • Always cover sharp edges.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?