BQT6904800 -03

Avoid Condensation

To maintain the specific insulation level, its crucial to shield the switchgears, particularly insulation parts, from condensation exposure.

Follow the below instructions to help avoid condensation:

  • Check the cubicles for any condensation. If any condensation is found, clean the cubicle and insulating components.

  • Inspect the cubicle for sufficient ventilation and heating. If required, use de-humidification devices.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?