BQT6904800 -03

Range of VDIS Unit Variants

For each version of VDIS unit, there are several variants (depending if it includes VO option or not). These variants can be identified as follows:

Table 9 Range of VDIS Unit Variant

VDIS unit variant

Reference

No VO

VDIS006STD

VO FlairDIN

VDIS007STD

Select the variants based on the following criteria:

  • The range of MV for the selected product.

  • The value of capacitor used inside the bushings of cubicle system.

  • The network frequency.

  • Associated devices.

Identifying Unit Parts

The VDIS unit consists of two sub-assemblies:

  • A protection sub-assembly with open seal.

  • An indication sub-assembly.

Keep the wiring set that is currently inserted in the existing unit. Disassembling the existing unit is required to recover the wiring set and assemble it into the new VDIS unit.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?