Withdrawable VT Operation
DANGER |
|---|
|
Hazard of electrical shock, explosion, or arc flash
Before opening the cable door ensure the following:
Failure to follow these instructions will result in death or serious injury.
|
CAUTION |
|---|
|
Hazard of Falling
Ensure the ramp is securely positioned and locked into
the panel before extracting the VT.
Failure to follow these instructions can result in injury or equipment damage.
|
Extraction of Withdrawable VT - With Transport Locks
Follow the below steps to remove the withdrawable VT from the cable compartment:
-
Open the door (1) of the cable compartment.
-
Position the ramp (2) correctly, and securely for the removal of the withdrawable VT truck (8).
Figure 59
Access to the Withdrawable VT1
Door
2
Ramp
-
Remove the bolts (4), washers (5), bolts (7), and washers (6) from the two transportation locks (3) using an Allen key.
Figure 60
Remove the Transportation Locks3
Transportation lock
6
Washer M8 x 4
4
Bolt M10 x 2
7
Bolt M8 x 4
5
Washer M10 x 2
-
Remove the transportation locks (3).
-
Carefully pull out the withdrawable VT truck (8) from the cable compartment.
Figure 61
Position the Withdrawable VT8
Withdrawable VT
-
Remove the withdrawable VT truck (8).
Insertion of Withdrawable VT
DANGER |
|---|
|
Hazard of electrical shock, explosion, or arc flash
The withdrawable VT truck must be locked into the cable
compartment.
Failure to follow these instructions will result in death or serious injury.
|
CAUTION |
|---|
|
Hazard of Falling
Ensure the ramp is securely positioned and locked into
the panel before extracting the VT.
Failure to follow these instructions can result in injury or equipment damage.
|
Follow the below steps to insert the withdrawable VT truck to the cable compartment:
-
Position the ramp (1) correctly and securely to insert the withdrawable VT truck into the cable compartment.
-
Carefully push the withdrawable VT truck (2) into the cable compartment.
-
On the withdrawable VT truck (2), push the hook (3), and the handles (4) down to lock it in the locking slot (5).
Figure 62
Insertion of withdrawable VT1
Ramp
4
Handle
2
Withdrawable VT
5
Locking slot
3
Hook
Extraction of Withdrawable VT - Without Transportation Locks
Follow the below steps to extract the withdrawable VT if the transportation locks does not exist:
-
Position the ramp correctly and securely for the removal of the withdrawable VT truck.
-
On the withdrawable VT truck (3), push the hook (1), and lift the handles (2) up to unlock it from the service position.
-
Carefully pull out the withdrawable VT truck (3) from the cable compartment.
Figure 63
Position the Withdrawable VT1
Hook
3
Withdrawable VT
2
Handle
-
Remove the withdrawable VT truck (3).
DANGER
CAUTION