BQT6904800 -03

Operations

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
  • Maintenance work must only be performed by trained electricians with proven experience of the MCSeT and all the relevant safety standards.
  • Comply with the operating sequences. Refer to Operations.
  • Perform every switching operation completely.
  • Ensure the presence of voltage in the system
  • After each switching operation that involves the use of a crank, lever, or handle, take out the tool and place it back in the transport trolley. Refer to Operation Accessories.
Failure to follow these instructions will result in death or serious injury.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?