BQT6904800 -03

Coupling Busbar Sections via BSC

With EvoPacT HVX Truck

Initial Situation:

  • VCB: OFF

  • EvoPacT HVX truck: In disconnected/test position

  • E/S: OFF

Coupling the Sections

Follow the steps for coupling the sections:

  1. Move trucks into the connected/service position (1).

  2. Switch ON the VCB (2).

Figure 51
Coupling Busbar Sections via BSC and EvoPacT HVX Trucks

Uncoupling

Follow the steps for uncoupling the sections:

  1. Switch OFF the VCB.

  2. Move trucks into disconnected/test position.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?