BQT6904800 -03

Maintenance Specifications

The MCSeT series indoor switchgear units are designed for normal operating conditions in accordance with IEC 62271-1. Refer to Safety Provisions.

For details, it is recommended contact our Schneider Electric service centre to help ensure correct functioning of the installation and maintenance.

After 6 to 12 months of operations, we recommend to check the busbars and MV cable connection tightening.

NOTE:
  • Check the power connections like busbars, cable connections and fixed contacts with a calibrated torque spanner.

  • Compare the values indicated and adjust if required. Refer to Screw Fastenings.

The elastic washers placed on the external sides of the connections and busbars helps to ensure better distribution of stress induced by the screw torque.

If no problems are detected, the busbars and cable connections are not modified, it is not necessary to do again this check. In case of dismantling, discard the removed elastic washers and install new elastic washers supplied by Schneider Electric.

Our service centre is at your disposal at any time:

  • To undergo an installation diagnostic.

  • To offer you, if need be, suitable maintenance operations.

  • To offer you maintenance contracts.

  • To offer you adaptations.

Inspection

DANGER
HAZARD OF ELECTRIC SHOCK, EXPLOSION OR ARC FLASH
In case of frequent condensation or air pollution (dust, smoke, or corrosive gases), the maintenance intervals must be adapted to the actual conditions.
Failure to follow these instructions will result in death or serious injury.

It is recommended to check the cubicles visually at regular intervals depending on the strain they are subject to during operation and in accordance with the national regulations.

A visual inspection includes a complete check of the cubicles by certified staff for contamination, condensation and damage.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?