BQT6904800 -03

Lubrication Instructions

NOTICE
HAZARD OF INAPPROPRIATE MAINTENANCE
The bearings and joints must not be washed out by the cleaning agent and following elements must not be lubricated:
  • Ball bearings
  • Auxiliary releases
  • Push switches
  • Auxiliary switches
Only approved lubricants may be used.
Failure to follow these instructions can result in equipment damage.

Preparation:

  1. Remove the truck from the panel.

  2. Clean lubrication points using a lint-free cloth, Refer to Figure 88.

    NOTE: Use cleaning agent in case of serious contamination.
  3. Use cleaning agents sparingly. Lubricating points must only be moistened. Refer to Auxiliary Products.

Figure 88
Lubrication points in the cubicle

A

Fixed contacts

D

VT Fuse

B

E/S contacts

E

Shutter mechanism

C

E/S operating mechanism

   
NOTE:
  • The lubricants are provided by the manufacturer. The use of alternative lubricants is not permissible.

  • The image shown here is for illustration purpose only.

Table 20 Details of Lubrication

Lubrication points

Lubricants

Lubrication procedure

Markers on the view

Sliding electrical contact surfaces

AMBLYGON TA 15/2
”KLUBER” (white)

Apply a thin and uniform film of lubricant.

A, B

All accessible friction points and mechanical sliding surfaces

MOBILITH SHC 100 (red)

Clean lubrication points with lint free cotton cloth; apply a thin film of lubricant (for example, using a paintbrush).

C

All accessible friction points and mechanical sliding surfaces

ISOFLEX TOPAS L152
”KLUBER” (white)

Clean lubrication points with lint free cotton cloth; apply a thin film of lubricant (for example, using a paintbrush).

D, E

Once maintenance work is complete:

  1. Remove all the tools and auxiliary equipment used.

  2. Re-insert truck into the panel.

  3. Reposition covers, close doors and check switching functions.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?