I/F Cubicle
Figure 3
I/F Cubicle
|
1 |
LV compartment |
10 |
Switch OFF push button of EvoPacT HVX VCB |
|
2 |
HMI screen |
11 |
Rating plate |
|
3 |
P5 relay |
12 |
Access to spring charge |
|
4 |
VDIS |
13 |
Access to Rack-in/Rack-out |
|
5 |
PowerLogic PD100 |
14 |
Operator interface of the E/S |
|
6 |
EvoPacT HVX VCB compartment |
15 |
Label of E/S manual operating instruction |
|
7 |
Handle |
16 |
Position inspection window for cables from rear window and VT |
|
8 |
Position inspection windows of the withdrawable part |
17 |
Cable compartment |
|
9 |
Switch ON push button of EvoPacT HVX VCB |