DOCA0188ZH-03

ComPacT NSX100-250 - 配电保护

MicroLogic 5.2 E6.2 E 7.2 E 脱扣单元

MicroLogic  5.2E,  6.2E  7.2E

40–160 A

Reflex 脱扣

MicroLogic  5.2E,  6.2E  7.2E

250 A

Reflex 脱扣

MicroLogic 6.2 E (接地故障保护)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

这有帮助吗?