DOCA0275EN-01

Boolean Logic Commands

Overview

The custom logic editor uses the following boolean logic commands:

  • LOAD_K_BIT

  • LOAD_BIT

  • LOAD_TMP_BIT

  • LOAD_NV_BIT

  • LOAD_NOT_BIT

  • LOAD_NOT_TMP_BIT

  • LOAD_NOT_NV_BIT

  • AND_BIT

  • AND_TMP_BIT

  • AND_NV_BIT

  • AND_NOT_BIT

  • AND_NOT_TMP_BIT

  • AND_NOT_NV_BIT

  • OR_BIT

  • OR_TMP_BIT

  • OR_NV_BIT

  • OR_NOT_BIT

  • OR_NOT_TMP_BIT

  • OR_NOT_NV_BIT

  • SET_BIT

  • SET_TMP_BIT

  • SET_NV_BIT

  • SET_NOT_BIT

  • SET_NOT_TMP_BIT

  • SET_NOT_NV_BIT

LOAD_K_BIT

The LOAD_K_BIT command loads a constant Boolean value (0 or 1) into the 1-bit accumulator.

Arguments

Representation

1

LOAD_K_BIT KValue

Input arguments

Type

Range

Description

KValue

BOOL

0/1

A constant value

No output arguments.

LOAD_BIT

The LOAD_BIT command loads the Boolean value (0 or 1) of a register bit into the 1-bit accumulator.

Arguments

Representation

2

LOAD_BIT RegAddr BitNo

Input arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

No output arguments.

LOAD_TMP_BIT

The LOAD_TMP_BIT command loads the Boolean value (0 or 1) of a temporary register bit into the 1-bit accumulator.

Arguments

Representation

2

LOAD_TMP_BIT TmpReg BitNo

Input arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

No output arguments.

LOAD_NV_BIT

The LOAD_NV_BIT command loads the Boolean value (0 or 1) of a non-volatile register bit into the 1-bit accumulator.

Arguments

Representation

2

LOAD_NV_BIT NVReg BitNo

Input arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

No output arguments.

LOAD_NOT_BIT

The LOAD_NOT_BIT command:

  • Inverts the Boolean value (0 or 1) of a specified register bit, then

  • Loads the inverted value into the 1-bit accumulator.

Arguments

Representation

2

LOAD_NOT_BIT RegAddr BitNo

Input arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

No output arguments.

LOAD_NOT_TMP_BIT

The LOAD_NOT_TMP_BIT command:

  • Inverts the Boolean value (0 or 1) of a specified temporary register bit, then

  • Loads the inverted value into the 1-bit accumulator.

Arguments

Representation

2

LOAD_NOT_TMP_BIT TmpReg BitNo

Input arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

No output arguments.

LOAD_NOT_NV_BIT

The LOAD_NOT_NV_BIT command:

  • Inverts the Boolean value (0 or 1) of a selected non-volatile register bit, then

  • Loads the inverted value into the 1-bit accumulator.

Arguments

Representation

2

LOAD_NOT_NV_BIT NVReg BitNo

Input arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

No output arguments.

AND_BIT

The AND_BIT command makes a logical AND link between a register bit value and the accumulator content in logic memory:

  • If the 1-bit accumulator equals 1 and the linked register bit equals 1, the result of the AND process is also 1.

  • In all other cases the result of the AND process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

AND_BIT RegAddr BitNo

Input arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

No output arguments.

AND_TMP_BIT

The AND_TMP_BIT command makes a logical AND link between a temporary register bit value and the accumulator content in logic memory.

  • If the 1-bit accumulator equals 1 and the linked temporary register bit equals 1, the result of the AND process is also 1.

  • In all other cases the result of the AND process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

AND_TMP_BIT TmpReg BitNo

Input arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

No output arguments.

AND_NV_BIT

The AND_NV_BIT command makes a logical AND link between a non-volatile register bit value and the accumulator content in logic memory.

  • If the 1-bit accumulator equals 1 and the linked non-volatile register bit equals 1, the result of the AND process is also 1.

  • In all other cases the result of the AND process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

AND_NV_BIT NVReg BitNo

Input arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

No output arguments.

AND_NOT_BIT

The AND_NOT_BIT command inverts the Boolean value (0 or 1) of a specified register bit, then makes a logical AND link between it and the accumulator content in logic memory:

  • If the 1-bit accumulator equals 1 and the linked register bit equals 0, the result of the AND process is also 1.

  • In all other cases the result of the AND process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

AND_NOT_BIT RegAddr BitNo

Input arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

No output arguments.

AND_NOT_TMP_BIT

The AND_NOT_TMP_BIT command inverts the Boolean value (0 or 1) of a specified temporary register bit, then makes a logical AND link between it and the accumulator content in logic memory:

  • If the 1-bit accumulator equals 1 and the linked temporary register bit equals 0, the result of the AND process is also 1.

  • In all other cases the result of the AND process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

AND_NOT_TMP_BIT TmpReg BitNo

Input arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

No output arguments.

AND_NOT_NV_BIT

The AND_NOT_NV_BIT command inverts the Boolean value (0 or 1) of a selected non-volatile register bit, then makes a logical AND link between it and the accumulator content in logic memory:

  • If the 1-bit accumulator equals 1 and the linked non-volatile register bit equals 0, the result of the AND process is also 1.

  • In all other cases the result of the AND process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

AND_NOT_NV_BIT NVReg BitNo

Input arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

No output arguments.

OR_BIT

The OR_BIT command makes a logical OR link between a register bit value and the accumulator content in logic memory:

  • If the value of either the 1-bit accumulator or the register bit equals 1, the result of the OR process is also 1.

  • If the values of all compared bits equal 0, the result of the OR process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

OR_BIT RegAddr BitNo

Input arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

No output arguments.

OR_TMP_BIT

The OR_TMP_BIT command makes a logical OR link between a temporary register bit value and the accumulator content in logic memory.

  • If the value of either the 1-bit accumulator or the temporary register bit equals 1, the result of the OR process is also 1.

  • If the values of all compared bits equal 0, the result of the OR process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

OR_TMP_BIT TmpReg BitNo

Input arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

No output arguments.

OR_NV_BIT

The OR_NV_BIT command makes a logical OR link between a non-volatile register bit value and the accumulator content in logic memory.

  • If the value of either the 1-bit accumulator or the non-volatile register bit equals 1, the result of the OR process is also 1.

  • If the values of all compared bits equal 0, the result of the OR process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

OR_NV_BIT NVReg BitNo

Input arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

No output arguments.

OR_NOT_BIT

The OR_NOT_BIT command inverts the Boolean value (0 or 1) of a specified register bit, then makes a logical OR link between it and the accumulator content in logic memory:

  • If the value of either the 1-bit accumulator or the register bit equals 0, the result of the OR process is also 1.

  • If the values of all compared bits equal 0, the result of the OR process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

OR_NOT_BIT RegAddr BitNo

Input arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

No output arguments.

OR_NOT_TMP_BIT

The OR_NOT_TMP_BIT command inverts the Boolean value (0 or 1) of a specified temporary register bit, then makes a logical OR link between it and the accumulator content in logic memory:

  • If the value of either the 1-bit accumulator or the temporary register bit equals 0, the result of the OR process is also 1.

  • If the values of all compared bits equal 0, the result of the OR process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

OR_NOT_TMP_BIT TmpReg BitNo

Input arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

No output arguments.

OR_NOT_NV_BIT

The OR_NOT_NV_BIT command inverts the Boolean value (0 or 1) of a selected non-volatile register bit, then makes a logical OR link between it and the accumulator content in logic memory:

  • If the value of either the 1-bit accumulator or the non-volatile register bit equals 0, the result of the OR process is also 1.

  • If the values of all compared bits equal 0, the result of the OR process is 0.

The result is saved in the 1-bit accumulator.

Arguments

Representation

2

OR_NOT_NV_BIT NVReg BitNo

Input arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

No output arguments.

SET_BIT

The SET_BIT command sets the value of the 1-bit accumulator to a specified register bit.

Arguments

Representation

2

SET_BIT RegAddr BitNo

No input arguments.

Output arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

SET_TMP_BIT

The SET_TMP_BIT command sets the value of the 1-bit accumulator to a specified temporary register bit.

Arguments

Representation

2

SET_TMP_BIT TmpReg BitNo

No input arguments.

Output arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

SET_NV_BIT

The SET_NV_BIT command sets the value of the 1-bit accumulator to a specified non-volatile register bit.

Arguments

Representation

2

SET_NV_BIT NVReg BitNo

No input arguments.

Output arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

SET_NOT_BIT

The SET_NOT_BIT command sets the inverted value of the 1-bit accumulator to a specified register bit.

Arguments

Representation

2

SET_NOT_BIT RegAddr BitNo

No input arguments.

Output arguments

Type

Range

Description

RegAddr

UINT

0–9249

The register address

BitNo

UINT

0–15

The bit number

SET_NOT_TMP_BIT

The SET_NOT_TMP_BIT command sets the inverted value of the 1-bit accumulator to a specified temporary register bit.

Arguments

Representation

2

SET_NOT_TMP_BIT TmpReg BitNo

No input arguments.

Output arguments

Type

Range

Description

TmpReg

UINT

0–299

The temporary register number

BitNo

UINT

0–15

The bit number

SET_NOT_NV_BIT

The SET_NOT_NV_BIT command sets the inverted value of the 1-bit accumulator to a specified non-volatile register bit.

Arguments

Representation

2

SET_NOT_NV_BIT NVReg BitNo

No input arguments.

Output arguments

Type

Range

Description

NVReg

UINT

0–63

The non-volatile register number

BitNo

UINT

0–15

The bit number

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?