Inputs Blocks
Overview
The FBD editor uses various inputs blocks accessible through the bar in the Toolbox:
|
Block |
Description |
|---|---|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
|
Constant Bit Block
Constant Word Block
The
block is used to set other
blocks inputs values (0 to 65,535).
Register Bit In Block
The
block enables the reading and use of a register
bit value from LTMT
main unit registers.
Register Word In Block
The
block enables the reading and use of a register
value from LTMT
main unit registers.
Register NV Bit Block
The
block enables the reading
and use of a non-volatile register bit value.
Register NV Word In Block
The
block enables the reading
and use of a non-volatile register value.
Register Temp Bit In Block
The
block enables the reading
and use of a temporary register bit value.
Temp Word In Block
The
block enables the reading
and use of a temporary register value.