DOCA0275EN-01

Communication Setting

The Communication Setting window contains the communication parameters.

The parameters are divided into the following sub-sections:

  • Fieldbus Protocol Settings or Profibus Settings: This window contains the parameters for the network settings of the TeSys Tera system.

    NOTE: Fieldbus Protocol Settings or Profibus Settings are available when the Field bus Protocol is selected as Modbus or PROFIBUS respectively.

  • Communication Loss: This window contains parameters to configure the communication loss settings.

  • HMI Communication: This window contains the parameters for the network settings of the LTMTCUF control operator unit.

  • HMI Communication Loss: This window contains parameters to configure the communication loss settings of the LTMTCUF control operator unit.

  • Device Session Management: This window contains parameter to configure the device session time out.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?