DOCA0275EN-01

Math Logic Commands

Overview

The custom logic editor uses the following math commands:

  • ON_ADD

  • ON_SUB

  • ON_MUL

  • ON_DIV

ON_ADD

The ON_ADD command performs unsigned addition when the 1-bit accumulator transitions from 0 to 1. It adds the value from Argument 1 to the 16-bit accumulator value, then posts the result back to the value in Argument 1.

Status register:

  • Indicates an overflow if the result of the addition process exceeds 65,535

  • Indicates the status of the 1-bit-accumulator from the previous scan

Arguments

Representation

2

ON_ADD TmpReg1 TmpReg2

Input Argument

Type

Range/Bit

Description

TmpReg1

UINT

0–65,535

Value to add to the 16-bit accumulator

Output Argument

Type

Range/Bit

Description

TmpReg1

UINT

0–65,535

Result of the addition operation

TmpReg2

UINT

Bit0

Overflow: the result of the addition is greater than 65,535.

In this case, the result of the addition is equal to Argument 1 + 65,536.

Bit3

1-bit accumulator history bit

ON_SUB

The ON_SUB command performs unsigned subtraction when the 1-bit accumulator transitions from 0 to 1. It subtracts the 16-bit accumulator value from the value in Argument 1, then posts the result back to the value in Argument 1.

Status register:

  • Indicates an underflow if the result of the subtraction process is less than 0

  • Indicates the status of the 1-bit-accumulator from the previous scan

Arguments

Representation

2

ON_SUB TmpReg1 TmpReg2

Input Argument

Type

Range/Bit

Description

TmpReg1

UINT

0–65,535

Value to subtract from the 16-bit accumulator

Output Argument

Type

Range/Bit

Description

TmpReg1

UINT

0–65,535

Result of the subtraction operation

TmpReg2

UINT

Bit0

Underflow: the result of the subtraction is less than 0.

In this case, the true result of the operation equals the value output to Argument 1 - 65,536.

Bit3

1-bit accumulator history bit

ON_MUL

The ON_MUL command performs unsigned multiplication when the 1-bit accumulator transitions from 0 to 1. The ON_MUL procedure multiplies the value from Argument 2 against the 16-bit accumulator value, then posts the result back to Argument 1 (most significant word) and Argument 2 (least significant word).

Status register indicates the status of the 1-bit accumulator from the previous scan.

Arguments

Representation

3

ON_MUL TmpReg1 TmpReg2 TmpReg3

Input Argument

Type

Range/Bit

Description

TmpReg2

UINT

0–65,535

Value to be multiply with the 16-bit accumulator

Output Argument

Type

Range/Bit

Description

TmpReg1 and TmpReg2

UINT

0–65,535

Result of the multiplication operation:

  • TmpReg1 holds the most significant word

  • TmpReg2 holds the least significant word

TmpReg3

UINT

Bit3

1-bit accumulator history bit

ON_DIV

The ON_DIV command performs unsigned division when the 1-bit accumulator transitions from 0 to 1. The ON_DIV procedure divides the combined value of Argument 1 and Argument 2 by the 16-bit accumulator value, then posts the result back to Argument 1 (most significant word) and Argument 2 (least significant word).

Status register indicates:

  • An overflow if division is by 0

  • The status of the 1-bit accumulator from the previous scan

Arguments

Representation

3

ON_DIV TmpReg1 TmpReg2 TmpReg3

Input Argument

Type

Range/Bit

Description

TmpReg1 and TmpReg2

UINT

0–65,535

Value to be divided by the 16-bit accumulator

Output Argument

Type

Range/Bit

Description

TmpReg1 and TmpReg2

UINT

0–65,535

Result of the division operation:

  • TmpReg1 holds the most significant word

  • TmpReg2 holds the least significant word

TmpReg3

UINT

Bit0

Division by 0

Bit3

1-bit accumulator history bit

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?