Display Options
Summary
You can customize the following display options to suit your requirements:
-
Zoom
-
Links
-
Arguments
Zoom Display Options
To access zoom options, select .
Three options are offered:
-
Zoom out to see more of the program at once.
-
Zoom in to focus on the program in more detail.
-
Zoom to 50%, 75%, 100%, 150 %, 200%, or 400% to have a customized view of the program.
Links Display Options
To access links display options, select .
Three options are offered. You can:
-
Renumber links, to aid in understanding the execution of the program.
-
Show all links, to see which blocks are linked together.
-
Hide all links, to have a better overall view of the blocks.
When you click on a link, its properties window appears and enables you to customize the text that appears next to the link.
Arguments Display Options
The following procedure describes how to access and change argument display options: