DOCA0275EN-01

Connecting the LTMT Main Unit to PC

The LTMT main unit can be connected to the PC running SoMove software in the following ways:

  • Connecting the USB port of the PC running SoMove software to the RJ45 on the LTMTCUF control operator unit using the USB/RJ45 cable for configuration and firmware update (recommended).

  • Connecting the USB port of the PC running SoMove software to the HMI port on the LTMT main unit using the USB/RJ45 cable for configuration and firmware update.

  • Connecting the USB port of the PC running SoMove software to the fieldbus port for configuration.

A Expansion module port (EXP)
B HMI port (HMI)

For more information on configuring the various communication protocol and establishing the connection between the TeSys Tera system and DTM library, refer to section Connection in the SoMove Online Help.

For more information on connecting the PC to the TeSys Tera system with LTMTCUF control operator unit, refer to TeSys Tera Motor Management System LTMTCUF Control Operator Unit User Guide – DOCA0233EN.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?