DOCA0275EN-01

Workspace Appearance and Graph Options

Summary

The FBD editor enables you to customize the workspace by changing its appearance and graph options.

Appearance and Graph Options

To access appearance and graph options, left-click anywhere in the workspace, except on an object.

Appearance Options

The following table lists all the possible appearance customization options:

Appearance option

Description

Possible choices

Background Color

Enables you to set the background color of the workspace by clicking the box where the color is displayed.

Choose between the colors available in the Custom, Web, and System tabs.

Background Type

Enables you to set the background type.

Choose between a flat color, gradient, or image background.

Enable Context Menu

Shows or hides the context menu.

True or False

Enable Tooltip

Shows or hides tooltips.

True or False

Restrict to Canvas

Enables you to choose whether the FBD program should be kept inside the canvas.

True or False

Show Grid

Enables you to choose whether the accurate grid is visible.

True or False

NOTE: This grid must not be confused with the grid line, which is accessed from the top-level View menu bar.

Graph Options

The following table lists all the possible graph customization options:

Graph option

Description

Possible choices

Allow Add Connection

Enables you to choose whether connections can be added to the workspace.

True or False

Allow Add Shape

Enables you to choose whether blocks can be added to the workspace.

True or False

Allow Delete Shape

Enables you to choose whether blocks can be deleted.

True or False

Allow Move Shape

Enables you to choose whether blocks can be moved in the workspace.

True or False

Locked

Enables you to choose whether the FBD program can be edited.

True or False

Display Gridlines

You may wish to display the grid lines. In order to do so, select Device > FB Diagram > View > Show Gridlines.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?