Pin Management
The Pin Manager secures the device by allowing you to set a pin on SoMove software.
The Pin Manager can be accessed by navigating to .
-
The Pin Manager is available only when the device is connected to SoMove software.
-
Pin Manager functionality is supported for the Ethernet variants if the LTMT main unit is connect through serial interface (HMIPort).
The following actions can be performed under the Pin Manager:
-
Create Pin
-
Modify Pin
-
Remove Pin
Creating a Pin
The Create Pin option allows you to create a new pin. The Create Pin option is available only when a pin is not set.
The following procedure shows how to create a pin:
-
Navigate to
.Result: The Create Pin dialog appears.
-
Enter a new six digit numeric pin in the New Pin and Confirm Pin fields.
-
Select Create.
Result: The pin is created.
You can set the session time using the Device Session Timeout parameter in the tab, a minimum of 5 minutes and a maximum of 60 minutes is allowed for each session.
Select Logout to disconnect the device from SoMove software.
Modify Pin
The Modify Pin option allows you to modify the pin. The Modify Pin option is available only after a pin is set.
The following procedure shows how to modify the pin:
-
Navigate to
Result: The Modify Pin dialog appears.
-
Enter the values for the Old Pin, New Pin, and Confirm New Pin respectively.
-
Select Modify.
Result: The pin is modified.
Delete Pin
The Remove Pin option allows you to delete the existing pin. The Remove Pin option is available only after a pin is set.
The following procedure shows how to remove the pin:
-
Navigate to
Result: The Remove Pin dialog appears.
-
Enter the existing pin in the Pin field.
-
Select Remove.
Result: The pin is removed.
Forgot Pin
In the event of forgetting the pin, a factory reset should be performed using the Reset button available on the device.