DOCA0275EN-01

General Settings

The General Settings window contains the general settings of the TeSys Tera system.

The following sub-sections are available:

  • Name Plate: Contains the name plate parameters.

    @Updated Draft 5
    NOTE: Changing the Load Type or Number of Phases and saving the settings will result in a device reboot.
  • Device Configuration: Contains the LTMT main unit temperature settings.

  • System Setting: Contains the current, voltage, phase rotation, nominal frequency, and mode parameters.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?