DOCA0275EN-01

My Dashboard

Overview

The My Dashboard tab allows you to customize data to configure or monitor based on requirement. It is used to:

  • Display the real-time value of the starter related parameters.

  • Display the information of input/output terminals.

  • Configure the starter and motor related parameters.

  • Configure the protection functions parameters.

NOTE: My Dashboard settings can be saved using Save Project option. The settings are retained if you save the project and open the saved project.

Description

The working space is divided into two zones:

  • Display zone: Displays the real-time value of starter parameters and status of input/output terminals for analysis.

  • Settings zone: Set the starter and motor parameters.

A Monitoring
B Settings
C Motor
D I/O terminals

Monitoring

The Monitoring area allows you to monitor the required parameters.

Settings

The Settings area allows you to monitor and change the protection function parameter values as per requirement.

The parameters under the Settings area can be assigned the required values by using the drop-down list.

Motor

The Motor area allows you to monitor and change the motor parameter values as per requirement.

I/O Terminals

The I/O Terminals area allows you to monitor the status of the I/O signals.

The following table describes the status of the input/output of the LTMT main unit and LTMT expansion modules with digital inputs or outputs.

Status input/output

Color status box

Descriptive text

Active

Green

Indicates that the IO terminal is assigned and active.

Inactive

Grey

Indicates that the IO terminal is assigned and not active.

Adding Parameters

The following procedure shows how to add parameters:

  1. Select icon in the area under which parameters need to be added.

    Result: The Select Parameter dialog appears.

  2. In the All Parameters column, select the required parameters and select the Right arrow. The search bar can be used to find parameters available under the All Parameters column.

    Result: The parameters are moved to the Selected Parameters column.

  3. To reorder the list of parameters, select the required parameter in the Selected Parameters column and select Up/Down arrow.

  4. Select OK.

The parameters added are displayed in the respective display area.

Deleting Parameters

To remove a parameter from an area, select icon in front of the parameter.

The following procedure shows how to remove multiple parameters:

  1. Select icon in the area under which parameters need to be removed.

    Result: The Select Parameter dialog appears.

  2. In the Selected Parameters column, select the required parameter and select the Left Arrow.

    Result: The parameters are moved to the All Parameters column.

  3. Select OK.

The parameters are removed from the respective display area.

NOTE: The list of parameters is configurable only under Settings and Motor areas.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?