DOCA0275EN-01

User Interface Description

The working space is divided into the following zones:

A

Menu bar

B

Tool bar

C

Status bar

D

Tab selection bar

E

Tab zone (content depending on the selected tab)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?