CALL_EOM Command Description
Overview
The CALL_EOM function allows to run an operating mode.
For this purpose, the function uses the temporary registers at addresses from 0 to 61.
To build a customized program around the CALL_EOM function, it is necessary to understand how the
different registers of the application and the LTMT
main unit are used:
-
Temporary registers at addresses from 25 to 29 are the input registers of the
CALL_EOMfunction. When customized, they must be assigned bit per bit. -
Temporary register at address 31 is the output register of the
CALL_EOMfunction. Its value is given after the execution of the operating mode. -
Temporary register at address 32 is a temporary register used to set the custom logic DO input information register at address 1291 (0x050B) in one time. The customization of the
CALL_EOMoutputs must be done using the temporary register at address 32.
Digital Input Registers
|
Register address |
Register description |
Bit |
Bit description |
|
5629 (0x15FD) |
Digital input register |
0 |
Local-START> DI |
|
1 |
Local-STOP DI |
||
|
2 |
Local-START>> DI |
||
|
3 |
Mode selection 1 |
||
|
4 |
Local-START< DI |
||
|
5 |
Local-START<< DI |
||
|
6 |
Remote-START> DI |
||
|
7 |
Remote-STOP DI |
||
|
8 |
Remote-START>> DI |
||
|
9 |
Mode selection 2 |
||
|
10 |
Remote-START< DI |
||
|
11 |
Remote-START<< DI |
||
|
12 |
Run DI |
||
|
13 |
Speed change DI |
||
|
14 |
Reserved |
||
|
15 |
Reserved |
HMI Input Registers
|
Register address |
Register description |
Bit |
Bit description |
|
9875 (0x2693) |
HMI command register 1 |
0 |
Motor run forward/High speed forward command |
|
1 |
Motor run reverse/High speed reverse command |
||
|
2 |
Local/Remote mode selection 1 |
||
|
3 |
Trip reset command |
||
|
4 |
Local/Remote mode selection 2 |
||
|
5 |
Self-test (without trip) command |
||
|
6 |
Motor low speed forward command |
||
|
7 |
Motor low speed reverse command |
||
|
8 |
Reset Inhibit command |
||
|
9 |
Reset number of starts command |
||
|
10 |
Reset number of stops command |
||
|
11 |
Clear energy command |
||
|
12 |
Reserved |
||
|
13 |
Logic test command |
||
|
14 |
Reset run hour command |
||
|
15 |
Self-test (with trip) command |
||
|
9876 (0x2694) |
HMI command register 2 |
0 |
Reserved |
|
1 |
Reserved |
||
|
2 |
Clear thermal capacity level command |
||
|
3 |
Reserved |
||
|
4 |
Reserved |
||
|
5 |
Clear trip counter command |
||
|
6 |
Factory reset command |
||
|
7 |
Soft starter reset command |
||
|
8–12 |
Reserved |
||
|
13 |
Store reference start curve command |
||
|
14 |
Clear trip records command |
||
|
15 |
Clear event records command |
Communication Input Registers
|
Register address |
Register description |
Bit |
Bit description |
|
704 (0x02C0) |
Communication command register 1 |
0 |
Motor run forward/High speed forward command |
|
1 |
Motor run reverse/High speed reverse command |
||
|
2 |
Local/Remote mode selection 1 |
||
|
3 |
Trip reset command |
||
|
4 |
Local/Remote mode selection 2 |
||
|
5 |
Self-test (without trip) command |
||
|
6 |
Motor low speed forward command |
||
|
7 |
Motor low speed reverse command |
||
|
8 |
Reset Inhibit command |
||
|
9 |
Reset number of starts command |
||
|
10 |
Reset number of stops command |
||
|
11 |
Clear energy command |
||
|
12 |
Motor Stop command |
||
|
13 |
Logic test command |
||
|
14 |
Reset run hour command |
||
|
15 |
Self-test (with trip) command |
||
|
705 (0x02C1) |
Communication command register 2 |
0 |
Reserved |
|
1 |
Reserved |
||
|
2 |
Clear thermal capacity level command |
||
|
3 |
Reserved |
||
|
4 |
Reserved |
||
|
5 |
Clear trip counter command |
||
|
6 |
Factory reset command |
||
|
7 |
Soft starter reset command |
||
|
8–12 |
Reserved |
||
|
13 |
Store reference start curve command |
||
|
14 |
Clear trip records command |
||
|
15 |
Clear event records command |
CALL_EOM 12 Description
When the CALL_EOM argument equals 12, the function
executes the overload operating mode.
The logic ID to use in your customized program is:
-
LOGID_ID 268 for overload operating mode
The temporary registers are used as follows:
|
Register |
Register description |
Bit |
Bit description |
|
Input register 25 |
Copy of the DI inputs |
0-15 |
Not used |
|
Input register 27 |
Copy of the HMI inputs |
0-15 |
Not used |
|
Input register 28 |
Copy of the communication inputs |
0-15 |
Not used |
|
Output register 31 |
Outputs of the |
0 |
Custom logic “Run1 Cde” information |
|
1-15 |
Not used |
||
|
Output register 32 |
Outputs of the |
0 |
Custom logic DO1 Input information |
|
1-15 |
Not used |
CALL_EOM 13 Description
When the CALL_EOM argument equals 13, the function
executes the Direct Online operating mode.
The logic ID to use in your customized program is:
-
LOGID_ID 269 for Direct Online operating mode
The temporary registers are used as follows:
|
Register |
Register description |
Bit |
Bit description |
|
Input register 25 |
Copy of the DI inputs |
0 |
Local-START> DI |
|
1 |
Local-STOP DI |
||
|
2 |
Not used |
||
|
3 |
DI Mode Selection 1 |
||
|
4-5 |
Not used |
||
|
6 |
Remote-START> DI |
||
|
7 |
Remote-STOP DI |
||
|
8 |
Not used |
||
|
9 |
DI Mode Selection 2 |
||
|
10-11 |
Not used |
||
|
12 |
Run DI |
||
|
13-15 |
Not used |
||
|
Input register 27 |
Copy of the HMI inputs |
0 |
HMI_START > |
|
1 |
Not used |
||
|
2 |
HMI_STOP |
||
|
3-4 |
Not used |
||
|
5 |
HMI Mode Selection 1 |
||
|
6 |
HMI Mode Selection 2 |
||
|
7-15 |
Not used |
||
|
Input register 28 |
Copy of the communication inputs |
0 |
COMM Start > |
|
1-3 |
Not used |
||
|
4 |
Remote Mode Selection 1 |
||
|
5 |
Remote Mode Selection 2 |
||
|
6 |
COMM Stop |
||
|
7-15 |
Not used |
||
|
Output register 31 |
Outputs of the |
0 |
Custom logic “Run1 Cde” information |
|
1-15 |
Not used |
||
|
Output register 32 |
Outputs of the |
0 |
Custom logic DO1 Input information |
|
1–15 |
Not used |
CALL_EOM 14 Description
When the CALL_EOM argument equals 14, the function
executes the Reverse Direct Online operating mode.
The logic ID to use in your customized program is:
-
LOGID_ID 270 for Reverse Direct Online operating mode
The temporary registers are used as follows:
|
Register |
Register description |
Bit |
Bit description |
|
Input register 25 |
Copy of the DI inputs |
0 |
Local-START> DI |
|
1 |
Local-STOP DI |
||
|
2 |
Not used |
||
|
3 |
DI Mode Selection 1 |
||
|
4 |
Local-START< DI |
||
|
5 |
Not used |
||
|
6 |
Remote-START> DI |
||
|
7 |
Remote-STOP DI |
||
|
8 |
Not used |
||
|
9 |
DI Mode Selection 2 |
||
|
10 |
Remote-START< DI |
||
|
11 |
Not used |
||
|
12 |
Run DI |
||
|
13-15 |
Not used |
||
|
Input register 27 |
Copy of the HMI inputs |
0 |
HMI_START > |
|
1 |
Not used |
||
|
2 |
HMI_STOP |
||
|
3 |
HMI_START < |
||
|
4 |
Not used |
||
|
5 |
HMI Mode Selection 1 |
||
|
6 |
HMI Mode Selection 2 |
||
|
7-15 |
Not used |
||
|
Input register 28 |
Copy of the communication inputs |
0 |
COMM Start > |
|
1 |
Not used |
||
|
2 |
COMM Start < |
||
|
3 |
Not used |
||
|
4 |
Remote Mode Selection 1 |
||
|
5 |
Remote Mode Selection 2 |
||
|
6 |
COMM Stop |
||
|
7-15 |
Not used |
||
|
Output register 31 |
Outputs of the |
0 |
Custom logic “Run1 Cde” information |
|
1 |
Custom logic “Run2 Cde” information |
||
|
2-15 |
Not used |
||
|
Output register 32 |
Outputs of the |
0 |
Custom logic DO1 Input information |
|
1 |
Custom logic DO2 Input information |
||
|
2-15 |
Not used |
CALL_EOM 15 Description
When the CALL_EOM argument equals 15, the function
executes the Star Delta operating mode.
The logic ID to use in your customized program is:
-
LOGID_ID 271 for Star Delta operating mode
The temporary registers are used as follows:
|
Register |
Register description |
Bit |
Bit description |
|
Input register 25 |
Copy of the DI inputs |
0 |
Local-START> DI |
|
1 |
Local-STOP DI |
||
|
2 |
Not used |
||
|
3 |
Mode Selection 1 |
||
|
4-5 |
Not used |
||
|
6 |
Remote-START> DI |
||
|
7 |
Remote-STOP DI |
||
|
8 |
Not used |
||
|
9 |
Mode Selection 2 |
||
|
10-11 |
Not used |
||
|
12 |
Run DI |
||
|
13-15 |
Not used |
||
|
Input register 27 |
Copy of the HMI inputs |
0 |
HMI_START > |
|
1 |
Not used |
||
|
2 |
HMI_STOP |
||
|
3-4 |
Not used |
||
|
5 |
Mode Selection 1 |
||
|
6 |
Mode Selection 2 |
||
|
7-15 |
Not used |
||
|
Input register 28 |
Copy of the communication inputs |
0 |
COMM Start > |
|
1-3 |
Not used |
||
|
4 |
Remote Mode Selection 1 |
||
|
5 |
Remote Mode Selection 2 |
||
|
6 |
COMM Stop |
||
|
7-15 |
Not used |
||
|
Output register 31 |
Outputs of the |
0 |
Custom logic Run1 command information |
|
1 |
Custom logic Run2 command information |
||
|
2 |
Custom logic Run3 command information |
||
|
3-15 |
Not used |
||
|
Output register 32 |
Outputs of the |
0 |
Custom logic DO1 Input information |
|
1 |
Custom logic DO2 Input information |
||
|
2 |
Custom logic DO3 Input information |
||
|
3-15 |
Not used |