DOCA0275EN-01

Inserting FBD Blocks

Overview

To create an FBD program, insert blocks into the workspace, then link them together. All types of blocks can be placed in the workspace.

Inserting Blocks from the Toolbox

The following procedure describes how to insert a block from the toolbox into the workspace:

  1. Select Device > FB Diagram > View > Toolbox or select the Toolbox tab on the left side.

  2. Select the type of block to insert:

    • Computation

    • Inputs

    • Function Blocks

    • Logic

    • Starter Types

    • Outputs

  3. Left-click on the icon corresponding to the block to insert.

  4. Drag and drop the block from the toolbox to the workspace.

  5. Position the block in the required location on the workspace.

  6. Repeat steps 2 to 5 to insert all the blocks required for the program.

Inserting Blocks from the Workspace

The following procedure describes how to insert a block directly from the workspace:

  1. Right-click anywhere on a blank space in the workspace.

    Result: A menu appears and enables you to select the type of block you want to insert.

  2. Select the type of block to insert:

    • Computation

    • Inputs

    • Function Blocks

    • Logic

    • Starter Types

    • Outputs

  3. Left-click on the block you want to insert.

  4. Position the block in the required location in the workspace.

  5. Repeat steps 1 to 5 to insert all the blocks required for the program.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?