Selecting Blocks
Overview
When you add blocks to the workspace, you can select them to reposition them within the workspace.
Selecting One or More Blocks
The following table describes how to select one or more blocks:
|
If you would like to select... |
Then |
|---|---|
|
An isolated block |
Click block. |
|
Several contiguous blocks |
Frame the blocks to be selected by defining a selection zone. |
|
Several blocks in different areas of the workspace |
Press the SHIFT key, then click the blocks to be selected while continuing to hold down the SHIFT key. Result: All of the selected blocks are highlighted with an orange outline. |
|
All objects including wires |
Select NOTE: The keyboard shortcut CTRL+A can also be used to select
all objects.
|