DOCA0275EN-01

Tab Zone

Overview

The table below lists the various tabs available.

@Updated Draft 5

Tab name

Description

My Device

Displays the device modules and characteristics.

Parameters List

Displays the configurable parameters of all device modules.

Settings

NOTE: The Settings tab is available only when the Ethernet variant of the LTMT main unit is selected in the My Device tab

Displays the configurable Modbus TCP and EtherNet/IP settings of the LTMT main unit.

My Dashboard

Displays the configurable and status parameters of all device modules, which can be customize based on the requirement.

Diagnostic

Displays diagnostic status data.

Monitoring

Displays the device modules monitoring data.

Start Curve

Displays the motor starting characteristics in a graphical format.

Custom Logic

Gives access to the custom logic editor of customized programs in custom logic language.

FB Diagram

Gives access to the custom logic editor of customized programs in FBD language.

Logic Simulator

Gives access to the logic simulator of customized programs in custom logic language.

Description

The window displays the common information in these tabs:

A Tree view
B Search function
C Display area
D Expand and Collapse buttons

Tree View

The tree view comprises of the parameter groups divided as items and sub-items. Select an item or a sub-item in the tree to display the parameter on the display area.

Search Function

The following steps describe how to find a specific text in the displayed table:

  1. In the first field of the search bar, enter the characters to search for (part of word, code, or unit).

  2. Select the column to search from the drop-down list.

    If you select the All option, the search is performed in all columns of the table.

  3. Select Search:

    • The first matching text found is highlighted.

    • To search for other instances, select Search.

    • If no matching text is found, the color of characters in the search field turns red.

Display Area in Grid View

A Column header
B Parameter group
C Parameters:
  • One parameter per row with parameter properties displayed in different fields.

  • Content of white cells can be modified, gray cells are read-only.

D Collapse or Expand icon: To collapse or expand a parameter group, click the arrow of the corresponding group.

Sorting Parameters

To sort the parameters according to the values in a column, click on the header:

Action

Result

Header Example

Single click

  • Parameter values are sorted in ascending order.

  • Header appears with an arrow pointing upwards.

Double click

  • Parameter values are sorted in descending order.

  • Header appears with an arrow pointing downwards.

Triple click

  • Parameters are displayed in their initial order.

  • Header appears according to its initial representation.

Modifying the Order of Columns

The following steps describe how to modify the order of columns in the display area:

  1. Click the header of the column.

  2. Drag the column to the desired location.

Expand and Collapse Button

The view of the display area can be modified using the following buttons available on the top right corner of the display area:

Button

Function

Description

Expand All

Expand all groups to display all parameters.

Collapse All

Collapse all groups in the display area.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?