DOCA0275EN-01

FBD Blocks Properties

Overview

Each of the blocks has a properties window. To display this window, left-click on a block.

The Properties window consists of several tabs, separated in 1 or 2 categories, depending on the type of block:

  • General settings, which contain the block ID and comments (common to all types of blocks.

  • Specific settings, depending on the type of block (register settings for registers, counter settings for counters, and so on.).

For example, if you want to display non-volatile register properties, select a non-volatile register block and left-click on it. The following window is displayed:

Comments

In the Comment zone, in the white box on the right of comments, you can enter a comment. Select any object or any free location in the workspace to save the comment.

Settings

Most blocks have a specific settings tab. In this tab, set the specific settings of blocks. These settings are described in detail in the help for each of the FBD blocks.

Properties Display

The properties of each block can be displayed in two different ways:

  • By category, clicking or

  • By alphabetical order, clicking .

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?