Definitions
Device Type Manager
The Device Type Manager (DTM) is a software module hosted in an FDT container for a specific device.
The functions of the DTM include:
-
Install device libraries
-
Update device libraries
-
Scanning various field buses for devices
-
Device power and energy monitoring
-
Management of configuration of device parameters
-
Project file management
-
Customizing of device parameter units
-
Troubleshooting
-
Update the firmware of device
SoMove Software Project File
A SoMove software project file is a configuration file for a pre-determined device, that can be created offline and saved for later use.
A project file contains the following information:
-
Device topology configuration
-
All parameters settings
-
The project file does not contain the customized program (custom logic program) and should be saved manually.
-
This file is saved with the extension *.psx.
For more information on how to create a project, refer to SoMove Online Help.