Monitoring
Overview
The Monitoring tab displays the monitoring of information related to the TeSys Tera system.
The monitoring information for the following categories are displayed:
-
Metering
-
Load Status
-
I/O Status
-
User Map
-
Custom Monitoring
Metering
The Metering window displays the metering data of the TeSys Tera system.
The metering signals are divided into the following categories:
-
Current
-
Voltage
-
Power
-
Energy
-
Temperature
-
Harmonics
-
My Device tab
-
-
Load Status
The Load Status window displays the load status of the TeSys Tera system.
The parameters under the load status page are divided into the following categories:
-
Motor
-
Thermal Memory
-
Statistics
-
Inhibit Status
The Load Status window also displays the total number of trips, inhibits, and alarms under Motor.
I/O Status
The I/O Status window displays the status of the analog and digital inputs and outputs of the TeSys Tera system.
The I/O signals are divided into the following categories:
-
Main Unit
-
Contactor Output
-
Expansion Module
User Map
The User Map window displays the live value of the parameters configured under section.
A maximum of 100 parameters are displayed.
Custom Monitoring
The Custom Monitoring window allows you to create a personalized monitoring window with widgets.
The signals are divided into the following categories:
-
Thermal
-
Current
-
Voltage
-
Power
-
Motor
Customizing the Custom Monitoring Window
The following procedure describes how to add a widget:
-
Select the signal to be monitored that are available under the available signal categories.
-
Click on the display area of the Custom Monitoring window.
Result: The Widget for the selected signal is added.
You can modify the widget display options by selecting option from the drop-down list.
To remove a widget from the display area, select
icon.
The following actions can be performed on the display area:
-
To remove all the widgets, right-click on the display area and select Clear All.
-
To organize the added widgets, right-click on the display area and select Arrange All.