DOCA0275EN-01

Installing TeSys Tera DTM Library

Overview

In SoMove software, a specific DTM exists for the TeSys Tera system. The TeSys Tera DTM Library must be installed after installing the SoMove software.

Downloading TeSys Tera DTM Library

TeSys Tera DTM Library can be downloaded from the Schneider Electric website (www.se.com)

Enter TeSys Tera DTM Library in the Search field to navigate to the downloads page.

NOTE: You must have administrator rights to install or uninstall the software on your PC.

Installing TeSys Tera DTM Library

The following steps describe installation of TeSys Tera DTM Library:

  1. Unzip the downloaded file TeSysTeraDTMLibrary.

  2. The folder will contain an exe file Schneider_Electric_TeSys_Tera_DTM_Library_V.X.Y.Z (where X.Y.Z is the version number) and a release note TeSysTeraDTMLibrary_vx.y.z_ReleaseNotes (where x.y.z is the version number).

  3. Double-click Schneider_Electric_TeSys_Tera_DTM_Library_V.X.Y.Z to start the installation.

  4. In the Choose Setup Language dialog, select the installation language and select OK.

  5. In the Welcome to the Installation Wizard for Schneider Electric TeSys Tera DTM Library dialog, select Next.

  6. In the Readme and Release Notes dialog, select Next.

  7. In the License Agreement dialog:

    • Read the license agreement carefully.

    • Select I accept the terms in the license agreement option.

    • Select Next.

  8. In the Customer Information dialog:

    • Enter the following information in the corresponding fields:

      • First name

      • Last name

      • Company name

    • Select Next.

  9. In the Destination Folder dialog:

    • If necessary, modify the TeSys Tera DTM Library destination folder by selecting the Change option.

    • Select Next.

  10. In the Ready to Install the Program dialog, select Install.

  11. In the Installation Wizard Completed dialog, select Finish.

    Result: The TeSys Tera DTM Library is installed on your PC.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?