DOCA0275EN-01

Starter Function Setting

The Starter Function Setting window contains the configurable parameters and options that control how the motor starter operates.

The parameters are divided into the following sub-sections:

  • Starter Setting: Contains adjustable parameters associated with the motor starter.

    @Updated Draft 5
    NOTE: Modifying the parameters under Starter Setting and saving the changes results in a device reboot.

  • I/O Setting: Contains the digital input and output settings of the LTMT main unit and LTMT expansion modules.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?