DOCA0275EN-01

FBD Resource Management

Overview

The LTMT main unit memory is equipped with the following resources:

  • 9250 LTMT registers

  • Logic memory space size equal to 8,192 words (16 bits)

  • 300 temporary registers

  • 64 non-volatile registers

Reserved Resources

The following table lists all reserved registers and their allocation. It also indicates how these registers are controlled:

Register type

Address range

Controlled by

Description

Temporary

0–69

User

Temporary storage of bit and registers assigned by you when creating an FBD program.

Temporary

70–299

FBD compiler

Reserved temporary registers for use by the compiler.

Non-volatile

0–31

User

Non-volatile bits or registers assigned by you when creating an FBD program.

Non-volatile

32–63

FBD compiler

Reserved non-volatile registers for use by the compiler.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?