DOCA0275EN-01

Custom Logic

Overview

The Custom Logic tab displays the custom logic editor which allows you to create a new custom logic program file or to open and edit any existing custom logic program file.

For more information about Custom Logic tab, refer to Custom Logic Editor

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?