DOCA0275EN-01

Parameters List

Overview

The Parameters List tab is used to define the parameter settings of the TeSys Tera system.

The parameter values can be modified in the Current Value field, both in connected and disconnected modes.

In connected mode, the settings can be updated to the device by selecting OK.

In disconnected mode, the configuration settings can be downloaded to the device by Store to Device operation.

NOTE: The values in the Parameter List tab are updated only once during initial loading. To view the updated values in the Parameter List tab in online mode, perform refresh operation.

Description

A Description: Name or Description of the parameter
B Current Value: Value of the parameter
C Wrench Mark: Appears if the current value is different from its default value
D Default Value: Default value of the parameter
E Min Value: Minimum value of the parameter
F Max Value: Maximum value of the parameter
G Address: Register address of the parameter

The following categories are available under the tree view in the Parameters Lists tab:

  • General Setting

  • Starter Function Setting

  • Protection Setting

  • Communication Setting

  • User Map

  • Modified Parameters

Setting Numerical Values

The numerical value of a parameter can be set in two ways:

  • Direct entry of the numerical value.

  • Value selection using the spin buttons

    .

The following steps describe how to set a numerical value by direct entry:

  1. Navigate to the required section under the tree view.

  2. Select a parameter from the list.

  3. Type the parameter value in the Current Value field.

  4. Select OK to write values to device in connected mode or to DTM offline configuration while in disconnected mode.

The following steps describe how to set a numerical value using the spin buttons:

  1. Navigate to the required section under the tree view.

  2. Select a parameter from the list.

  3. In the Current Value field, set the parameter value using the spin buttons.

  4. Select OK to write values to device in connected mode or to DTM offline configuration while in disconnected mode.

Editing a String

The following steps describe how to set a string parameter:

  1. Navigate to the required section under the tree view.

  2. Select a parameter from the list.

  3. Type the string in the Current Value field.

  4. Select OK to write values to device in connected mode or to DTM offline configuration while in disconnected mode.

Selecting Values in a List

The following steps describe how to select a value in a list:

  1. Navigate to the required section under the tree view.

  2. Select a parameter from the list.

  3. In the Current Value field, set the parameter value using the drop-down list.

  4. Select OK to write values to device in connected mode or to DTM offline configuration while in disconnected mode.

For a global description of the tab, refer to section Tab Zone description.

NOTE: After editing the default values from the parameters list and select OK, below warning message will appear. Ensure if the required measures are met, and select OK.
WARNING
Unintended Behavior of Equipment
  • Changing the Device Configuration can result in a short-circuit or turn on power supply to the load.
  • Check if the appropriate wiring and configuration is done according to the Device Configuration.
  • Ensure that the three phase power supply is cut off while changing the CTVT Sensor and Starter.
Failure to follow these instructions can result in death, serious injury, or equipment damage.

Important Information

  • The parameters available for configuration are based on the TeSys Tera system configuration. 

  • If the parameter values entered are invalid, an error message will be displayed. Read the message and set the values appropriately.

  • Store to Device operation cannot be performed when the motor is in run state.

  • By default, the Communication Loss protection function is disabled. If this function is enabled and the device is connected to the SoMove software through the Modbus RTU communication port, and if you try to disconnect the DTM, the communication loss trip will be triggered in the device.

  • Configuration of all setting under Parameters List, except for User Map, is disabled when the motor is in run state. In order to configure the parameters, stop the motor and then configure the settings.

  • For the alarm to be triggered before the pickup level, the Alarm Level parameter configuration should be less than or equal to the Trip Level parameter configuration.

  • When configuring the start and stop of the motor in a system as a single relay, the DI Start Validation Time should be greater than the DI Stop Validation Time.

  • To configure the parameters under the Fieldbus Protocol Setting, Profibus Settings, and HMI Communication sections, the device should be disconnected from the DTM. After performing a store to device operation to write the changed settings to the device, you can connect to the device by performing the Scan Devices using the new parameter values provided.

  • If the Main Unit Temperature value is set to None, Temperature Protection settings will be unavailable for configuration.

  • If LTMTCUF control operator unit is connected on HMI port. The HMI Communication Settings must be configured as follows:

    • Node Address: 1

    • Baud rate: 19200 bps

    • Parity: Even

    • Byte Format: Big Endian

  • If the Starter Type is configured as reversible, the Interlocking Time is not considered during a change of motor direction if the DI is selected as Forced Start.

  • For more information on the individual parameters, refer to TeSys Tera Motor Management System User Guide – DOCA0257EN.

  • The value in the Default Value column remains constant, regardless of any configuration changes.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?