My Device
Overview
tab is used to:
-
Configure the TeSys Tera system in disconnected mode.
-
Display the TeSys Tera system characteristics in connected mode.
Description
This figure presents the different sections of My Device tab.
| A | Main Unit |
| B | Main Unit CT Sensor Module |
| C | Configured Bill of Materials |
| D | Reference Mismatch |
| E | Expansion Modules |
Main Unit
The Main Unit section displays the information of the LTMT main unit configured in the TeSys Tera system.
The following characteristics are available in the Main Unit section:
|
Characteristics |
Description |
|---|---|
|
Name Tag |
Enter the name of the LTMT main unit. NOTE:
|
|
Reference |
Select the reference of the LTMT main unit. NOTE: LTMTEFM is selected as default LTMT
main unit reference.
|
|
Firmware Version |
Displays the firmware version of the selected LTMT main unit. NOTE: The firmware version is only displayed when the device
is online.
|
|
Field Bus Protocol |
Displays the used network protocol of the LTMT main unit. The following options are available to select for the Ethernet variants of the LTMT main unit:
|
Main Unit CT Sensor Module
The Main Unit CT Sensor Module section displays the information of the main unit CT sensor module configured in the TeSys Tera system.
The following characteristics are available in the Main Unit CT Sensor Module section:
|
Characteristics |
Description |
|---|---|
|
Name Tag |
Enter the name of the Main Unit CT Sensor Module. NOTE:
|
|
Reference |
Select the reference of the Main Unit CT Sensor Module. |
|
Current Range |
Displays the current range of the selected sensor module. |
|
Voltage Range |
Displays the voltage range of the selected sensor module. NOTE: The voltage range is displayed for the voltage variants only.
|
|
Firmware Version |
Displays the firmware version of the selected main unit CT sensor module. NOTE: The firmware version is only displayed when the device
is online.
|
|
CT Sensor Cable |
Select the type of sensor cable used. |
Expansion Module
The Expansion Module section displays the information of the expansion modules configured in the TeSys Tera system.
The following characteristics are available in the Expansion Module section:
|
Characteristics |
Description |
|---|---|
|
Name Tag |
Enter the name of the LTMT expansion module. NOTE:
|
|
Reference |
Select the reference of the LTMT expansion module. |
|
Firmware Version |
Displays the firmware version of the LTMT expansion module. NOTE: The firmware version is displayed when the device
is online.
|
|
Expansion Module Cable |
Select the reference of the cable used to connect the LTMT expansion module. |
Select Add Expansion Module card to add up to five LTMT expansion modules.
The following table depicts the maximum number of LTMT expansion modules that can be added in the TeSys Tera system:
|
LTMT expansion modules reference |
Maximum units |
|
LTMTIN42FM/LTMTIN42BD |
5 |
|
LTMTAN21 |
2 |
Reference Mismatch
The Reference Mismatch section shows the difference between the configured devices and the identified devices.
Configured Bill of Materials
The Configured Bill of Materials displays the list of all the devices and accessories configured in the TeSys Tera system.
Based on the configuration made for the TeSys Tera system, the list of the modules are displayed in a tabular format.
|
Characteristics |
Description |
|
Device Type |
Displays the type of device connected. |
|
Reference |
Displays the reference of the connected device or accessory. |
|
Serial Number |
Displays the serial number of the connected device. NOTE: The serial number is only displayed when the device is online.
|
|
Version |
Displays the version number of the connected device. NOTE: The version number
is only displayed when the device is online.
|
|
Quantity |
Displays the number of devices, CT Sensor Cable, and Expansion Module Cable used. |
The configured bill of materials can be exported as a CSV
file by selecting the (Export Bill of Materials) icon.